Abort_connection_option_code

Index.Sub

 6007.0H

Data Type Integer16
Access Read/Write
PDO Mappable

No

Unit --
Range

 0 = No action

 1 = Fault signal

 2 = Disable voltage command

 3 = Quick stop command

Default Value 0
Store Supported Yes
Description This object defines the reaction to be executed when a communication abort event is triggered.
Notes --